AXIS#.MT.DISALLOWZEROSTARTVEL

Description

This parameter sets the motion task control word specifying whether or not the starting velocity of the task can be 0.

It takes the following values:

Value Description
0

Non-zero start velocity disallowed

1 Non-zero start velocity allowed

Examples

Usage

This keyword is used to set what you would otherwise have set with AXIS#.MT.CNTL.

Code

MT.NONZEROSTARTVEL 0 1 Will configure Motion Task 0 to allow non-zero start velocity.

Context

See AXIS#.MT.CNTL for more information on the argument semantics.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write Array
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also AXIS#.MT.CNTL

Stored in Non-Volatile Memory

No

Variants Supported

Supported on all drives.